Accelerated graphics requirement

2024-05-20T23:35:28Z

Summary


Details

NX has always required accelerated graphics, which makes a graphical processing unit (GPU) essential when running NX.

Previously, if a GPU was not present, the session would still run and, depending on the commands that are used may even appear to have been a successful session. In those cases, a message would appear in the syslog file about the lack of a GPU being present, but the user often did not see this information, so it may have appeared that the GPU was only recommended, instead of required.

Advancements in the graphics libraries used in NX now require the use of a GPU.

Starting with the June 2023 release, if a GPU is not present NX displays the following message to the user, which is also written to the syslog file.

*******************************************************************                Graphics Configuration Error This is an unaccelerated graphics configuration. NX requires accelerated graphics configurations. Perhaps the graphics device is unsupported or perhaps an unsuitable device driver is installed. Attempt to open any part may result in program termination. *******************************************************************

If you ignore this message and continue to run the NX session, it could lead to undefined behavior or error messages.

The GPU requirement is for interactive or 'headless' image capture sessions. Other 'headless' NX batch sessions will continue to function as before.

Supported hardware and graphics

The list of currently supported hardware and graphics cards can be found on Hardware and Software Certifications.

https://support.sw.siemens.com/en-US/product/209349590/knowledge-base/PL8017193

Click NX-Graphics-Certification-Table to open a spreadsheet that has tabs for supported systems and graphics.

KB Article ID# PL8719836

Contents

SummaryDetails

Associated Components