How to machine a contoured hole

2023-05-30T11:23:13Z

Summary


Details

The requirement is to use a full radius T cutter to finish the interior of a hole or bore with contoured walls.  How can this be done?

Solution

We can use the fixed axis surface contouring operation type with a 'surface area' drive method to create smooth tool path on a simple drive surface and then project that path onto the more complex part faces.

KB Article ID# PL8719502

Contents

SummaryDetails

Associated Components