How to keep the set Unit of measure in Solid Edge Simulation?

2023-08-31T13:07:36Z

Summary


Details

In Solid Edge Simulation it is possible to change the Units. For example, Force from mN to N, and Pressure from kPa to Pa.

However, Solid Edge does not save the setting for the next part. 

How can the unit be set so that it can be subsequently used with other files?

Platforms
  • na windows-1064
Release Versions
  • Solid Edge V223UPD5
Solution

The Units are kept inside the template.

To change this for future use:

-Open 'Solid Edge Options'  and select the 'Units'

-Edit the Units you want

-'Save as' and rename the template to e.g "metric_part_Newton.par" and save it in the folder you use:

E.g. "C:\Program Files\Siemens\Solid Edge 2023\Template\Metric"

Next time you create a new part select the template you want to use.

Notes

KB Article ID# PL8719156

Contents

SummaryDetails

Associated Components