mom_attr_OPER_xxxxx - No NC Output

2023-05-30T11:21:54Z

Summary


Details

When assigning an attribute to an operation, that attribute is not outputting when postprocessing with Post Builder and using mom_attr_OPER_"attribute_name"  to output NC code.

Solution

TCL error occurred  with the properties set as seen below... the only value that output in the NC output was "CUSTOM_EPAC"


To correct the problem, the values of the properties on the operation had to be Upper Case. The properties set as seen below resulted in good NC output ...


KB Article ID# PL8719099

Contents

SummaryDetails

Associated Components