Using Move Object involving a Target and Tool body

2023-06-07T18:10:21Z

Summary


Details

Using Move Object involving a Target and Tool body

Platforms
  • na windows-1064
Release Versions
  • NX V2027
Solution

Development confirmed that when using Move Object with a feature involving a Target and Tool body, such as Trim and Extend, the Target will always move with the Tool, and the Tool is free to move independtley.  For example, if a Trim and Extend feature is not the current feature, the Tool body of the Trim and Extend feature is free to move, but if the Target is desired to move, the Trim and Extend feature will move with it. 

Notes

KB Article ID# PL8718812

Contents

SummaryDetails

Associated Components