Convert NX part from inch to mm in Teamcenter environment

2023-05-25T06:42:29Z

Summary


Details

We have a NX assembly which in general is built upon millimeter unit, but there are some components that have got the unit inch. Would now like to get away from a mixed units assembly and consolidate everything to millimeter part files.- How to run ug_convert_part utility in NX manager mode, i.e. in Teamcenter environment?

Platforms
    Release Versions
    • NX V12.0.2
    • NX V1847
    • NX V1872
    • NX V1899
    • NX V1953
    • NX V1980
    • NX V2007
    • NX V2206
    • NX V2212
    Solution

    ug_convert_part does not support a Teamcenter managed environment.

    Instead use the part_utility and its Teamcenter Integration for NX option -convert_units_to_mm, (there is also a -convert_units_to_in option for going in the opposite direction).

    Example running from a command prompt with necessary TC and NX variables set:
    Convert units to millimeters in a folder of parts:
             part_utility -managed_mode=yes -u=<user name> -p=<password> -f=<folder name in Teamcenter> -convert_units_to_mm

    Notes

    Ref NX 2212 documentation, (Teamcenter Integration for NX -> Utilities -> part_utility):
    https://docs.sw.siemens.com/en-US/doc/209349590/PL20220512394070742.tcint/xid1483665

    KB Article ID# PL8718772

    Contents

    SummaryDetails

    Associated Components