Enable Active Workspace to see and open previous saved version of UGMaster

2023-05-18T21:04:28Z

Summary


Details

In Teamcenter RAC, it is possible to open a previously saved version of UGMaster dataset via File > Open With...


How to configure Active Workspace to enable the same functionality to see and open previously saved version of UGMaster dataset?


Solution

Using Teamcenter RAC, go to Edit > Options...

Set up following two TC preferences:

(1) TC preference: AWC_StartupPreferences must contain this line of value called: AWC_NX_OpenOldDatasetVersionIsEnabled


(2) TC preference: AWC_NX_OpenOldDatasetVersionIsEnabled must be set to: true


Once the TC preferences are set, the function is executed by:

(1) Open the Item Revision in Active Workspace

(2) Activate the Attachements Tab

(3) Select the UGMASTER or UGPART dataset

(4) In Active Workspace: Right hand side vertical Panel > Open > Open in NX...

(4a) In NX embedded: Right hand side vertical Panel > NX > Open in NX...

Notes

When using Open With... to load a previously saved version of a dataset, do not use the Assembly Load Options "Minimally Load - Lightweight Display".


KB Article ID# PL8717683

Contents

SummaryDetails

Associated Components