What is the Command Sequence Definition File used for in Customer Defaults?

2023-06-07T18:09:56Z

Summary


Details

What is the Command Sequence Definition File used for in Customer Defaults?


Solution

The Command Sequence Definition File is used for creating scripts or journals to run a series of commands which can be named and called upon to run that series of commands.  Please use the provided link to the NX Documentation on using a Command Sequence Definition File.

https://docs.sw.siemens.com/en-US/doc/209349590/PL20200605195244930.nx_interface/xid1929524

KB Article ID# PL8717320

Contents

SummaryDetails

Associated Components