Solid Edge Solid Edge 2022 - Maintenance Pack 13 Announcement

2023-05-15T18:14:06Z
SE_BETA SE_TSS DOC_MANAGEMENT FLOEFD 3D-SKETCH SIMULATION Teamcenter Share TECH_PUB ASSEMBLY APPLICATION PART/SHEETMETAL TRANSLATORS DRAFT SETUP Solid Edge Marketing

Summary


Details

May 15, 2023

Dear Solid Edge Customer:

Solid Edge 2022 Maintenance Pack 13 is now available for download.

We appreciate your continued business and participation in the software support process - - your reporting helps us make Solid Edge more productive for how you do business.

Sincerely,

The Solid Edge Team

============

Release Notes:

============

Solid Edge 2022 MP13

Version: 222.00.13.04

Solid Edge 2022 Maintenance Packs are delivered using Microsoft Installer (MSI) technology.

Support Center: https://support.sw.siemens.com

===============

Email Notification:

===============

To receive direct email notifications for Solid Edge Maintenance Packs, navigate to your Support Center profile:

https://account.sw.siemens.com/profile, scroll down to Newsletter Subscriptions, then check the box for 

Software Field Bulletin

============================================

This Maintenance Pack addresses the following PRs:

============================================

===Assembly===

PR 10332389: Assembly cut feature fails when a user selects active body/Thru-next

PR 10630963: Cannot add points to Elec Routing path using the alt-click method

PR 10453306: Fastener System all lengths of screws in selection mask

PR 10473327: Harness parts not displaying on the screen

PR 10485964: DBAdmin entry fields delete button

PR 10619745: hiding an assembly group also hiding unrelated assemblies

PR 10624533: Update causing drawing issues

PR 10635919: Adjust parts lose their adjustable definitions

PR 10666435: Pipes/Frames and such disappear when unrelated asm feature/bodies are deleted

PR 10670397: Some parts with features do not reflect changes in top-level asm

PR 10467699: Impossible to edit Motion "Friction" values "Radius" and "Length

PR 10687440: Reproducible abort when entering variable names in the Variable Table

PR 8674428: Edit 3D sketch by single selection does not select segments

===Part/Profile/Sheetmetal===

PR 10606305: Cutout problem in sheetmetal

PR 10643558: Solid Edge crashes when performing certain actions in Sheetmetal.

PR 10691383: Making a sketch after Duplicate results in close

PR 10499398: Undo crash

===Translators===

PR 10462165: DXF created from Solid Edge disply layers that should be off

PR 10583794: Creo Elements Direct Data Migration fails: Cannot activate Part Library module

PR 10625063: Creo Assembly Files created are empty.

PR 10540497: Impossible to use ICF from Solid Edge 2022 MP11 in Tekla

KB Article ID# PL8717000

Contents

SummaryDetails

Associated Components

SE_BETA