Dear Siemens Digital Industries Software Customer,
We are pleased to inform you that Tecnomatix controllers for "FANUC_RJ, KUKA_KRC, KUKA_KRC_BMW"
are available for download from https://support.sw.siemens.com.
See Tecnomatix_Controller_Name_changes_log.htm for details concerning this update.
Note: This file is located in the 'OLP Change Logs' folder directly under the 'Process Simulate Robot Controllers' folder.
Use the following steps to download:
- Login to https://support.sw.siemens.com
- If you do not have an account, click 'Register Now' and fill out the information.
- Once on Support Center, if you do not see Tecnomatix under 'My Products', click 'Manage Products'.
- Scroll down and toggle On the Tecnomatix product.
- Scroll back to the top and click Support Center in the breadcrumb.
- Select 'Tecnomatix' from 'My Products'
- Select 'Download'
- Select 'Additional Downloads'
- Select 'Process Simulate Robot Controllers'
- Select 16.0, 16.1, 16.1.1, 16.1.2, 17.0, 2206 or 2301
[Or Select 'Older Versions' to access 15.1 or 15.1.2]
Download the file(s):
Tecnomatix_15.1_FANUC_RJ_64BIT_v3.84.1_09_05_2023.exe
Tecnomatix_15.1_KUKA_KRC_64BIT_v6.0.3_09_05_2023.exe
Tecnomatix_15.1_KUKA_KRC_BMW_64BIT_v4.18.8_09_05_2023.exe
Tecnomatix_15.1.2_FANUC_RJ_64BIT_v3.84.1_09_05_2023.exe
Tecnomatix_15.1.2_KUKA_KRC_64BIT_v6.0.3_09_05_2023.exe
Tecnomatix_15.1.2_KUKA_KRC_BMW_64BIT_v4.18.8_09_05_2023.exe
Tecnomatix_16.0_FANUC_RJ_64BIT_v3.84.1_09_05_2023.exe
Tecnomatix_16.0_KUKA_KRC_64BIT_v6.0.3_09_05_2023.exe
Tecnomatix_16.0_KUKA_KRC_BMW_64BIT_v4.18.8_09_05_2023.exe
Tecnomatix_16.1_FANUC_RJ_64BIT_v3.84.1_09_05_2023.exe
Tecnomatix_16.1_KUKA_KRC_64BIT_v6.0.3_09_05_2023.exe
Tecnomatix_16.1_KUKA_KRC_BMW_64BIT_v4.18.8_09_05_2023.exe
Tecnomatix_16.1.1_FANUC_RJ_64BIT_v3.84.1_09_05_2023.exe
Tecnomatix_16.1.1_KUKA_KRC_64BIT_v6.0.3_09_05_2023.exe
Tecnomatix_16.1.1_KUKA_KRC_BMW_64BIT_v4.18.8_09_05_2023.exe
Tecnomatix_16.1.2_FANUC_RJ_64BIT_v3.84.1_09_05_2023.exe
Tecnomatix_16.1.2_KUKA_KRC_64BIT_v6.0.3_09_05_2023.exe
Tecnomatix_16.1.2_KUKA_KRC_BMW_64BIT_v4.18.8_09_05_2023.exe
Tecnomatix_17.0_FANUC_RJ_64BIT_v3.84.1_09_05_2023.exe
Tecnomatix_17.0_KUKA_KRC_64BIT_v6.0.3_09_05_2023.exe
Tecnomatix_17.0_KUKA_KRC_BMW_64BIT_v4.18.8_09_05_2023.exe
Tecnomatix_2206_FANUC_RJ_64BIT_v3.84.1_09_05_2023.exe
Tecnomatix_2206_KUKA_KRC_64BIT_v6.0.3_09_05_2023.exe
Tecnomatix_2206_KUKA_KRC_BMW_64BIT_v4.18.8_09_05_2023.exe
Tecnomatix_2301_FANUC_RJ_64BIT_v3.84.1_09_05_2023.exe
Tecnomatix_2301_KUKA_KRC_64BIT_v6.0.3_09_05_2023.exe
Tecnomatix_2301_KUKA_KRC_BMW_64BIT_v4.18.8_09_05_2023.exe
To Install:
Place Tecnomatix_<TecnomatixVersion>_<ControllerName>_NNBIT_vVV_MM_DD_YYYY.exe into a folder ($Tecnomatix/downloads is suggested, where $Tecnomatix is the full path to the Tecnomatix installation).
Run Tecnomatix_<TecnomatixVersion>_<ControllerName>_NNBIT_vVV_MM_DD_YYYY.exe.
The default installation point is C:\Program Files\Tecnomatix.
If you have any issues with the installation or support of these fixes,
please contact your local GTAC support group.
Sincerely,
Siemens Digital Industries Software