May 8, 2023
Dear Solid Edge Customer:
Solid Edge 2023 Update 0005 is now available for download.
We appreciate your continued business and participation in the software support process - - your reporting helps us make Solid Edge more productive for how you do business.
Sincerely,
The Solid Edge Team
============
Release Notes:
============
Solid Edge 2023 Update 0005
Version: 2210.0005.006 x64
Download Solid Edge 2023 (v2210) Updates
Note: if the direct download URL doesn't resolve in your browser, please navigate from the top-level Support Center.
===============
Email Notification:
===============
To receive direct email notifications for Solid Edge Updates, navigate to your Support Center Profile (https://account.sw.siemens.com/profile, scroll to Newsletter Subscriptions, and check the box for Software Field Bulletin.
==========================================
This Solid Edge Update resolves the following PRs:
==========================================
===Assembly===
PR 10373996: Peer locate is not working for block occurrence geometry
PR 10453306: Fastener System all lengths of screws in selection mask
PR 10473327: Harness parts not displaying on the screen
PR 10485964: DBAdmin entry fields delete button.
PR 10600009: The user is unable to mirror two features in this file
PR 10614240: The user is unable to show/hide swept protrusion features in PF
PR 10637289: The user is unable to create a subtract part feature on target that is overridden in the assembly
PR 10645903: Insert Assembly Issue causes an immediate abort
PR 10647258: Unable to select internal faces with Selection Manager
PR 10624533: Solid Edge 2023 Update 3 is causing drawing issues
PR 10663105: RMB click Accept not working Fastener System
PR 10598818: Assembly can be opened in Solid Edge 2022 MP11 but failed to open in 2023
PR 10630565: The user is unable to create a subtract part feature from the assembly
PR 10635919: Adjust parts lose their adjustable definitions
PR 10642360: Features disappear from the screen when the user deletes a failed feature
PR 10666435: Frames disappear when an unrelated assembly feature/body is deleted
PR 10670339: The user can create PWD features in new architecture files
PR 8627594: The user is not able to Trim/Extend a Frame
PR 10670397: Some parts do not update in the top-level assembly
PR 10687440: Reproducible abort when entering variable names in the Variable Table
PR 10702395: Unable to edit Thread created as assembly Feature
===Draft===
PR 10615750: Connector annotations cannot be deleted using the left click and delete key
===General===
PR 10597046: Some active command buttons are indistinguishable from inactive command buttons
PR 10679788: Solid Edge 2023 MP4 Major Crashing Issues
PR 272934: Backport UX enhancements
PR 285848: The Command Tool Box doesn’t Fade in and Fade out as expected in the Draft environment
===Part/Profile/Sheetmetal===
PR 10591992: Bad display of holes in wireframe display mode.
PR 10643558: Solid Edge crashes when performing specific actions in Sheetmetal.
PR 10678608: Can't create a Cutout
PR 10691383: Solid Edge will close after defining a sketch on duplicate features
===SEEC===
PR 10619277: Custom FOA properties not visible on the property form
PR 10452908: FOA is slow when saving in Teamcenter
===Translators===
PR 10462165: DXF created from Solid Edge display layers that should be off
PR 10540497: Impossible to use ICF from Solid Edge 2022 MP11
PR 10326074: IFC-Import - Lots of Parts missing
PR 8675718: Wrong Helical Curve Lead angle due to high tolerance
PR 10691626: Unable to export ground constraints from Solid Edge Motion to NX MCD