How to Add an Attribute Column to the Assembly Navigator

2024-03-07T16:00:25Z

Summary


Details

 How to add a column in the Assembly Navigator to display a specific attribute.

Solution

 See the above video showing how to add a column to the Assembly Navigator and display a specific attribute.

How to Add an Attribute to the Assembly Navigator

1.       Open the Assembly.

2.       Verify the desired properties are updated.

-          Note: Mass Properties can be verified using the Analysis tab -> Mass Properties group -> Show Mass Properties Panels. The Mass Properties table that appears in the Assembly navigator will show the current mass properties.

3.       In the Assembly Navigator, right click on the empty space beside the column headers.

4.       Choose Columns -> Configure.

5.       In the Assembly Navigator Properties dialog, select the Columns tab and choose Attribute Column Selector.

6.       Locate the desired property and select it.

7.       Click OK.

8.       Click OK.

9.       The density is now displayed in the Assembly Navigator.

KB Article ID# PL8715142

Contents

SummaryDetails

Associated Components