Unable to check-mate test multiple components detected in visual reporting at the same time

2023-05-08T02:21:13Z

Summary


Details

I gave the components the user attribute as per material type and detected it in Visual Reporting, but since I cannot select multiple results from the report window, I cannot test them similar (material) attributes at the same time.

Reproduced Steps:

1. Create User Defined Attributes/Attribute Values for Assembly Models

   P_MAT: classified into JA..., JP..., HC...


2. Color-coded display for each attribute/attribute value using Visual Reporting command

*** Reference: PL8714956 “Color-code display of components by user-defined attribute”

3. Trying to select multiple results in the search results window

*Multiple selection is not possible.


*For single selection is possible with selecting one result in the listing > right-click > "Send to" > "Execute Check-Mate Tests", though.

Solution

It's not possible to select multiple results in the visual report search results window. This behavior is working as designed.

WORKAROUND:

By using the component group function, you can deal with it by grouping reports in advance.

1. Assembly Navigator > “Component Groups in Parts” > “Match all of... component Group” > (As the group) put any name in the field


2. “Match all of...” > “Add to Component Group...” > complete the expression with put an attribute in “Name” and a attribute value in “Value” in the input field.



-- Creation Example --


3. HD3D tab > “Controls” > “Define New Report > After entering each items as follows, click "OK“



4. Select a component group listed in the result window > “Send To“ > “Execute Check-Mate Tests”


*** It can be sent by group (multiple components) into "Set Up Tests" dialog and tested it.


Notes

Regarding definition and others for User Define Attributes, please refer to the following documentation link.

https://docs.sw.siemens.com/en-US/doc/209349590/PL20220512394070742.properties_parts_objects/edt_prop_general_t

Also, regarding Visual Reporting command, please refer to the following documentation link.

https://docs.sw.siemens.com/en-US/doc/209349590/PL20220512394070742.xid895105/hd3d_visrpt_ov

Also, regarding Check-Mate command, please refer to the following documentation link.

https://docs.sw.siemens.com/en-US/doc/209349590/PL20220512394070742.checkmate/xid1649740

***Please refer to PL8714958 for Japanese article.

Release Versions
  • NX V11.0.2
  • NX - DESIGN V11.0.2
Platforms

    KB Article ID# PL8714960

    Contents

    SummaryDetails

    Associated Components