Color-code display of components by user-defined attribute

2023-05-08T02:01:31Z

Summary


Details

Components in an assembly have certain attributes attached to it. Its attribute values vary from component to component. For example, if material attributes are defined by the user, is it possible to display them in different colors using the attributes/attribute values?

Reproduced Steps:

1. Create user-defined attributes/attribute values for each component

e.g, P_MAT: Giving component attributes/attribute values such as JA..., JP...


Solution

Using the visual report function, you can color-code display for each attribute/attribute value.

1. HD3D tools tab > Visual Reporting

2. Controls > define new report

*** E.G, the setting contents in the dialog are the reference in the red frame.



Notes

For more information on creating user-defined attributes, please refer to the documentation link below.

https://docs.sw.siemens.com/en-US/doc/209349590/PL20220512394070742.properties_parts_objects/edt_prop_general_t

For more information on Visual Reporting, please refer to the following document link.

https://docs.sw.siemens.com/en-US/doc/209349590/PL20220512394070742.xid895105/hd3d_visrpt_ov

***Please refer to PL8714955 for Japanese article.

Release Versions
  • NX V11.0.2
  • NX - DESIGN V11.0.2
Platforms
  • Windows x64 10

KB Article ID# PL8714956

Contents

SummaryDetails

Associated Components