W scale in text command cannot be fixed (e.g, To 100%)

2023-05-08T01:50:09Z

Summary


Details

In Text command to input as a curve, if specifying the length and height when inserting or editing, the W scale will change according to those specified values, and the aspect ratio cannot be fixed (for example, 100%).

Reproduced Steps:

1. Menu > Insert > Curve > Text


2. Specify( or change) Length or Height


Solution

The behavior is working as expected. If either length or height is specified, the W scale will be changed according to these settings.

Workaround:

After specifying the height, specify the desired W scale (e.g 100%).

Notes

An option to fix the W scale is planned to be enhanced in NX 2312.

***Please refer to PL8714949 for Japanese article.

Release Versions
  • NX V2027
  • NX - DESIGN V2027
Platforms

    KB Article ID# PL8714950

    Contents

    SummaryDetails

    Associated Components