How to select from list of available naming rules to assign ID in NX

2023-05-03T13:14:31Z

Summary


Details

In NX during File New creation, how to select from a list of mulitple available Naming Rules that are attached to a certain item type?

This is possible in Teamcenter with an item type having multiple Naming Rules configured, to choose from the multiple available Naming Rule to use:


How to achieve the same result using NX File->New command?

Solution

In NX during the File New dialog, place cursor over the field for ID, and do Right Mouse Button. Notice the popup dialog shows all the available Naming Rules. The one with check mark is the active Naming Rule.


Notes

To configure multiple naming rule on an item type, see following Teamcenter documentation:

https://docs.sw.siemens.com/en-US/doc/282219420/PL20220523331910052.plm00071/c03a004

KB Article ID# PL8714919

Contents

SummaryDetails

Associated Components