'Additive Manufacturing' tab is missing in NX Managed Mode

2023-05-01T12:21:20Z

Summary


Details

NX/TC Managed Mode does not display the 'Additive Manufacturing' tab when selecting File-New

Solution

The following steps were taken to enable 'NX Fixed Plane Additive Manufacturing Integration'.

·        Opened the 'Environment Manager' from the Windows Start menu.


·        Installation using TEM to install the feature 'NX Fixed Plane Additive Manufacturing Integration'.


·        Opened the TC Command Prompt and set UGII_TMP_DIR, UGII_TEMP_DIR and PATH.

Please see sample below…


·        Locate the file below and drag it into your TC Command Prompt window .                           Please see sample below.

C:\Program Files\Siemens\NX2212\UGII\templates\sample\tcin_fpam_template_setup.bat -u=password -p=password

Note: You’ll need to add the -u and -p (username and password) and have admin rights to run the file.

KB Article ID# PL8714348

Contents

SummaryDetails

Associated Components