Warning 3025001 when using the utility ug_clone

2023-09-18T10:04:30Z

Summary


Details

The utility "%UGII_BASE_DIR%\NXBIN\ug_clone.exe is not working as expected and the following warning is shown:

Warning: (3025001) - The Clone operation has not been initialised

Platforms
  • na windows-1064
Release Versions
  • NX V2212
  • NX V2306
Solution

The utility ug_clone is sensitive to the order of the arguments and the general advice is to use the arguments in the order listed via the -help flag or as specified in the documentation (Teamcenter Integration for NX - Run ug_clone).

For example:

"%UGII_BASE_DIR%\NXBIN\ug_clone.exe" -pim=yes -u=**** -p=**** -g=**** -o=export -asse=@DB/000614/A -default_n=autotranslate -default_d=c:\temp\export

Notes

KB Article ID# PL8713234

Contents

SummaryDetails

Associated Components