Installing Structure Designer Library in Teamcenter environment with NX 2212

2023-04-20T23:44:48Z

Summary


Details

Where is the Structure Designer Library installation tool located in NX 2212?

(In previous NX release, it was located in the UGII_BASE_DIR\ NXSTRUCTUREDESIGN\InstallationTool\StructureDesignerLibraryInstallation folder)

Solution

Starting from NX 2212, NX is consolidating most of the library install tools into one common folder location. This includes Structure Designer tools.

In NX 2212 and newer, please use nx_library_installation.exe located in UGII_BASE_DIR \DESIGN_TOOLS\library_installation


This install tool consolidates various different library installs together under the same tool:


The Structure Designer installation guide is available to download from this article:

Instruction_Library_Installation_Tool_v1.0.docx (2.93 MB)

KB Article ID# PL8713166

Contents

SummaryDetails

Associated Components