How to Edit the Extension Lines of Drafting Dimensions

2024-03-07T15:58:04Z

Summary


Details

How to Edit the Extension Lines of Drafting Dimensions.

Solution

See the above video showing how to edit the extension lines of drafting dimensions.

How to Edit the Extension Lines of Drafting Dimensions

1.       Open the Drawing.

2.       Double click on the desired dimension.

3.       A small square will appear where the dimension line meets the View. Click on it.

4.       In the pop-up menu, the following can be manipulated:

-          Extension Line visibility.

-          Jog presence.

-          Distance between extension line and its point of measurement.

5.       To alter both Extension Lines simultaneously, click on the button with two purple arrows.

6.       Click Close.

KB Article ID# PL8712094

Contents

SummaryDetails

Associated Components