NX Mass properties do not update in navigator after material change

2023-04-12T07:42:50Z
NX for Design

Summary


Details

Show Mass Properties Panels does not update the Mass and Weight when another material (different density) is assigned to a solid.

Measure the Solid body does show correct values.

Platforms
  • INTL64 windows-1064
Release Versions
  • NX V1946
Solution

Add the solids to the System Reference Set (probably "Model").

This case the Solid bodies where not part of "Model" reference set, which is used for assign weight. The System Reference Set is defined in customer default.

Notes

KB Article ID# PL8711084

Contents

SummaryDetails

Associated Components

Modeling