Cutting a Vertical Wall Using a Floor Wall Operation

2023-04-18T17:20:03Z

Summary


Details

The radiused corner of a block needs to be milled off. 


A 2D Profile Wall without Floor operation is selected and the 3D IPW option is set so that the tool only cuts where material is still present.


Notice the remaining material in the picture below.


The operation is set up and generated. A message is reported that the Part cannot be faced at any level. What settings need to be changed to get this to work?


Platforms
  • INTL64 windows-1064
Release Versions
  • NX V2206.8100
Solution

To get this operation to run go to Options -> All other Parameters and  turn on the Extend Floor to Blank Outline and the Cut Pattern Follow Part.


Notice that the tool only cuts where needed.


Notes

KB Article ID# PL8710708

Contents

SummaryDetails

Associated Components