How to fix the size of sketch dimension without depend on the view scale factor

2023-04-10T23:34:04Z

Summary


Details

When I zoom in or out the view in the sketch environment, the size of the sketch dimension is scaled depending on the view scale. Is there any way to fix the size on the screen?

Solution

Can be controlled by Customer Defaults or Sketch Settings. Please set “Fixed Text Height on Screen" to "ON".

Customer defaults

File > Utilities > Customer Defaults > Sketch > General > Sketch Settings


Preferences

File > Preferences > Sketch > Sketch Settings


Notes

This setting has no effect on existing sketch features. In addition, the change for each feature can be controlled by Part Navigator > Select a sketch feature > Settings.


***Please refer to PL8709748 for Japanese article.

Release Versions
  • NX V2212
Platforms
  • Windows x64 10

KB Article ID# PL8709749

Contents

SummaryDetails

Associated Components