The geometries are enlarged after copy/paste

2023-04-03T04:05:07Z

Summary


Details

Copying the geometries (edges, etc.) displayed in the drawing view and pasting them to the drawing sheet, but they are generated in actual size. Is it possible to generate (copy & paste) the same length?

Reproduced Steps:

1. Create a drawing view with any scale such as 1/5.

2. Select some geometries > Click mouse light button > “Copy”


3. In Drawing sheet, click mouse light button > “Paste”


Solution

The behavior is working as expected.

Workaround:

Able to get the expected result by pasting in the same drawing view (or a view with the same scale).

Copy & Paste in the same drawing view:


Notes

***Please refer to PL8709315 for Japanese article.

Release Versions
  • NX V2000
  • NX - DRAFTING V2000
Platforms

    KB Article ID# PL8709316

    Contents

    SummaryDetails

    Associated Components