Use Functional Mockup Unit (FMU) in Process Simulate

2023-05-16T13:43:25Z

Summary


Details

How to import a Functional Mockup Unit (FMU) into Process Simulate

Solution

Steps to import a FMU into Process Simulate:

1) Export the FMU from an external program (i.e. OpenModellica)


2) Copy the exported file (*.fmu) into the FMI Vault under the Process Simulate Installation Location. The default path should be  ...\Tecnomatix_<Version_Nr>\emPower\Scripting\FMI\Vault


3) Extract the *fmu file into the Vault folder. This creates a folder containing the model and the library components 

4) Open Process Simulate to use the FMU in the SCL-Editor. (Note: Before the FMU can be used all instances of Process Simulate have to be closed)


KB Article ID# PL8709095

Contents

SummaryDetails

Associated Components