Dear Siemens Digital Industries Software Customer,
We are pleased to inform you that Tecnomatix External Connections for "Rockwell Automation, Mitsubishi Electric"
are available for download from https://support.sw.siemens.com.
Use the following steps to download:
- Login to https://support.sw.siemens.com
See "Tecnomatix Mitsubishi V1.0 Manual" and "Tecnomatix Rockwell V1.0 Manual" for more information regarding the applications.
Note: This file is located in the 'OLP Change Logs' folder directly under the 'Process Simulate Robot Controllers' folder.
- If you do not have an account, click 'Register Now' and fill out the information.
- Once on Support Center, if you do not see Tecnomatix under 'My Products', click 'Manage Products'.
- Scroll down and toggle On the Tecnomatix product.
- Scroll back to the top and click Support Center in the breadcrumb.
- Select 'Tecnomatix' from 'My Products'
- Select 'Download'
- Select 'Additional Downloads'
- Select 'Process Simulate External Connections'
- Select 'Process Simulate External Connections Mitsubishi' or 'Process Simulate External Connections Rockwell'
Download the file(s):
Tecnomatix Mitsubishi V1.0 Beta.msi
Tecnomatix Rockwell V1.0 .msi
To Install:
Place Tecnomatix <Name> <Version>.msi into a folder ($Tecnomatix/downloads is suggested, where $Tecnomatix is the full path to the Tecnomatix installation).
Run Tecnomatix <Name> <Version>.msi.
The default installation point is C:\Program Files\Tecnomatix.
If you have any issues with the installation or support of these fixes,
please contact your local GTAC support group.
Sincerely,
Siemens Digital Industries Software