No.
While the default resolution can be defined, the pixel and print dimensions are calculated based on the input CGM size so cannot be set by default. Unlike a plotter format which has sheets and rolls upon which you can scale plots to fit, image output formats do not have this capability.