Solid Edge Define a part occurrence with a precision of 0.001 m

2023-08-09T09:55:54Z
PART/SHEETMETAL

Summary


Details

In a Solid Edge assembly with a non-graphic part, the occurrence is specified in meters.  I would like to define a precision of 0.001m instead of 0.01m.

How to define this?

Platforms
  • na windows-1064
Release Versions
  • Solid Edge V223.0
Solution

You must separate the unit type and decimal places with a semi-colon (;).  If the number of decimal places you want is 2, you do not need to enter a value for the decimal places.

The solution is to modify the custom property defined for the non-graphic part:

SE_ASSEMBLY_QUANTITY_STRING -> meters;3

Notes

KB Article ID# PL8707502

Contents

SummaryDetails

Associated Components

PART/SHEETMETAL: FLAT_PATTERN