Symbol Library folders are not displayed

2024-05-13T16:44:45Z

Summary


Details

When creating a custom symbol in Drafting, the Symbol Library folders are not displayed on the Reuse tab of the Resource Bar, or in the 'Define Custom Symbol' dialog box.

Solution

Turn ON the following Customer Default:

1. Select 'File-->Utilities-->Customer Default'.
2. Expand 'Gateway' and highlight 'Reuse Library'.
3. Select the 'Symbols Library' tab.
4. Set:  Display Symbol Library in Browser = ON
5. OK the 'Customer Defaults' dialog.
6. Re-start NX for the Customer Default to take effect.

Notes

KB Article ID# PL8707376

Contents

SummaryDetails

Associated Components