'Use simplified Assembly' and 'Use Designed Assembly' applied to main assembly only

2023-04-03T15:26:53Z

Summary


Details

In an assembly, when one toggles the main assembly to 'Use simplified Assembly' or 'Use Designed Assembly' this is applied to the main assembly only.

Solution

This is working as Designed.

In order to apply 'Use Simplified Assembly' or 'Use Designed Assembly' to all lower-level assemblies the user needs to hold the CNTRL key whilst clicking the command.

Notes

A PR existed for this functionality where it did not work in a mixture of designed and simplified subassemblies. That PR has since been solved with Solid Edge 2023 Update 2 and Solid Edge 2022 MP 12.

KB Article ID# PL8706966

Contents

SummaryDetails

Associated Components