NX Arrowhead end point of the linked PMI note points to a different position than the source part

2023-03-24T03:17:40Z
NX for Design

Summary


Details

I created PMI Note from the source part using the "WAVE PMI Linker" for the part created by "Create Linked Mirror Part". Even though the arrowhead end point in the source part is pointing on the face, that in the mirror part is not pointed on the face.

PS. In case of PMI Note automatically linked by "Create Linked Mirror Part" points correctly on the face.

Reproduced Steps:

1. Perform “Create Linked Mirror Part”


2. Delete “PMI Note” in the mirror part


3. Link the PMI Note in the source part into the mirror part


Result of WAVE PML Linker:


Solution

The behavior is due to NX problem and was fixed in NX 2212.

Workaround : not use “WAVE PMI Linker” and use “Create Linked Mirror Part”

Notes

The issue occurs in NX 2206 and lower Series.

And then it occurs with all commands in “Annotation” group such as PMI Note, Balloon, Feature Control Frame, Weld Symbol, Datum Feature Symbol and etc.

***Please refer to PL8705845 for Japanese article.

Release Versions
  • NX - PMI V1919
Platforms
  • Windows x64 10

KB Article ID# PL8705846

Contents

SummaryDetails

Associated Components

PMI