Export Parasolid, Selected Objects selection doesn't exclude unsupported objects

2023-03-17T12:18:14Z

Summary


Details

When doing Export Parasolid, using Model Data Export: Selected Objects option and selecting objects using a selection rectangle the message:


          "Object of unsupported type on export list"

Occurs when <OK> is pressed to execute the export. 

The export operation is not possible to execute at this point. This use to work in older NX versions.

- Why is this?

Platforms
  • na windows-1064
Release Versions
  • NX V2007
  • NX V2206
  • NX V2212
Solution

Export Parasolid functionality was enhanced in NX 2007 resulting in a new UI. This is why there is a difference in behavior between older versions and NX 2212.

Currently, when using Selected Objects option, please use the standard filter utility set to supported object types like Solid Body, Sheet Body etc. to ensure only valid object types are selected.


Notes

KB Article ID# PL8705663

Contents

SummaryDetails

Associated Components