Value changes when changing perpendicular dimension to cylindrical dimension

2023-03-24T03:14:06Z

Summary


Details

After creating a cylindrical dimension in the drafting environment using "Use Baseline" option, changing an existing Perpendicular dimension to a cylindrical dimension results in incorrect dimension value.

Reproduce Steps:

1. File > New and create Cylinder > go to Drafting and place a view新規

2. Create “Perpendicular” dimension


3. Create “Cylindrical” dimension with “Use Baseline” option


4. Change the perpendicular dimension created in the step 2 to a cylindrical dimension. (Select dimension > Right click mouse > Edit > Change to diameter dimension)


Solution

The behavior is due to NX problem and was fixed in NX 2212 Series.

Workaround: Recreate Cylindrical dimension without “Use Baseline" option.

Notes

The behavior occurs in NX 2206 and lower Series.

The issue occurs only in Perpendicular dimension.

***Please refer to PL8705207 for Japanese article.

Release Versions
  • NX V1946
  • NX - DRAFTING V1946.3700
Platforms
  • Windows x64 10

KB Article ID# PL8705208

Contents

SummaryDetails

Associated Components