"Internal error" occurs when creating a level task in BIM design

2023-03-24T03:12:57Z

Summary


Details

When entering the level task environment in BIM design and creating a line on the level, after specifying the first point, dragging the mouse cursor (holding down the left mouse button) and trying to select the second point, " Internal error: memory access violation" occurs.

Reproduced Steps:

1. File > New > BIM Design > select BIM Structure Assembly template > OK > OK

2. After select Level > Line, select the first point on the screen and drag the mouse cursor (hold down and move the cursor to select the second point)

*** “Internal Error : memory access violation” occurs



Solution

The behavior is due to NX problem and is fixed in NX 2306 Series.

Note that the data is not corrupted by the error and can be used continuously.

Notes

***Please refer to PL8705199 for Japanese article.

Release Versions
  • NX V2212
  • NX - BIM_DESIGN V2212
Platforms
  • Windows x64 10

KB Article ID# PL8705200

Contents

SummaryDetails

Associated Components