STEP export fails in managed mode

2024-05-13T16:53:17Z

Summary


Details

STEP file fails to export to a local folder from managed NX.

There are no errors in the NX log file. There is only an alert in NX:
  ==================
STEP242 Export Failed
@DB/Part1/A failed to export
==================  

Solution

Check the output file name for the number of characters in the entire "path + filename".
Are there more than 80 characters (including spaces)?
This could be an issue since there are character limits.Please export the STEP to a local folder that has a very short path and no spaces or special characters in the folder names.
Example: C:\users\Part1_A.stp

Notes

KB Article ID# PL8705042

Contents

SummaryDetails

Associated Components