Name of User Defined Feature not displayed in input browser

2023-03-24T03:11:35Z

Summary


Details

User Defined Feature Library browser does not display the name of registered library, sometimes partially or not at all.

Reproduced Steps:

1. Register a feature by User Defined Feature wizard

  Name = Test1

  Part Name = Part1


2. Launch User Defined Feature Library Browser

*** The name of the feature registered does not displayed.


Solution

The issue is due to NX problem and is fixed in NX 2206.6000.

Workaround : enlarge or reduce the dialog size.


In addition, when the control returns to the browser after inserting User Defined feature, the name is not displayed even if the size of the dialog is enlarged/reduced. In this case, restart the browser once.


Also, if the feature name is the same and the part name is different when registering User Defined feature, the name is not displayed even if the workaround is applied, so it is recommended to avoid creating feature with the same name.

Example created with Name=Test1, Part Name=Part2:


"Name" of "Part2" is not displayed:


Notes

The behavior occurs in NX 2007, 2206 and NX 2212 Series.

***Please refer to PL8705024 for Japanese article.

Release Versions
  • NX V2212
Platforms
  • Windows x64 10

KB Article ID# PL8705024

Contents

SummaryDetails

Associated Components