NX PMI Coordinate Note does not follow when rotating component

2023-03-24T03:05:27Z
NX for Design

Summary


Details

In the assembly environment, PMI Coordinate Note does not follow and are moved to an unintended location when the component is rotated.

Steps to Reproduce:

1. Create a component in a top assembly and PMI Coordinate Note in the component.


2. Open the top assembly and then rotate the component e.g. “Motion/Dynamic” in “Move Component”.

*** PMI Coordinate Note is moved to an unintended location.


Result:


Solution

The behavior is due to NX problem and is fixed in NX 2306 Series. There is no workaround, so Siemens would like you to use PMI Coordinate Note only when there is no rotational translation under the assembly.

Notes

The behavior occurs in NX 1872 - NX 2206.

The Behavior only occurs in PMI Coordinate Note. There is no problem with Note, General Note, Specific Note, etc.

Parallel movement of the component has no problem, it only happens with rotation.

In addition, when performing "Add Component", a problem also occurs if the component is moved by rotation.

***Please refer to PL8704930 for Japanese article.

Release Versions
  • NX V2015
Platforms
  • Windows x64 10

KB Article ID# PL8704951

Contents

SummaryDetails

Associated Components

PMI