Engage and Retract Options Missing on Variable Contour Dialog

2023-03-20T20:15:51Z

Summary


Details

A Variable Contour operation is created and is setup to get the desired tool path. When the Non Cutting Moves menu is expanded the Engage and Retract settings are missing. What happened to the Engage and Retract settings?



Platforms
  • na windows-1064
Solution

When the Non-Cutting Moves text was selected in older versions of NX the display did not change. In newer versions a menu is now visible.


Unchecking the Override With Smooth Connections option will cause the Engage and Retract menus to be available.


Notes

KB Article ID# PL8704882

Contents

SummaryDetails

Associated Components