Getting "NX Nastran Error" message when using Solid Edge Simulation.

2023-03-16T14:24:49Z

Summary


Details

Getting "NX Nastran Error" message when using Solid Edge Simulation creating a Mesh in SE2022. Several users of Solid Edge SE2022 with the latest Maintenance Packs have no issues when creating a Mesh within the Simulation environment; in this case, the user which is having the problem can go to other computers and get the same error message.

Platforms
  • all n/a-n/a
Release Versions
  • Solid Edge V222.0
Solution

 It is VERY likely this is related to the user's Windows Profile, but it may be difficult to isolate the actual reason for the problem. The easiest solution is to delete and recreate the Windows Profile. Contact your IT specialist for assistance.

Notes

KB Article ID# PL8704797

Contents

SummaryDetails

Associated Components