Solid Edge What are the certified platforms for Solid Edge FlexLM License server located in the Cloud?

2024-08-05T03:19:39Z
PART/SHEETMETAL SETUP

Summary


Details

If the customer sets up a FlexLM server in the Cloud, which platforms are certified?

Solution

The Amazon Cloud and Microsoft Azure both are permitted, certified platforms for Solid Edge FlexLM.

Notes

If you have further inquiries about floating Licensing please refer to the FAQs collection link below:

Solid Edge Floating License FAQs Collection


KB Article ID# PL8704785

Contents

SummaryDetails

Associated Components

PART/SHEETMETAL: FEATURES