In a Teamcenter integrated NX environment, how to display MBD Query rules

2023-03-28T11:53:43Z

Summary


Details

In a Teamcenter integrated NX environment, how to display MBD Query logical rules

Solution

To display the MBD Logical rules in Teamcenter integrated NX, you need to import them in Teamcenter database.

First  you need to set the desired Teamcenter location in the customer defaults as below.


So make sure to create the above folder in Teamcenter.

Now you need to import the logical rules in this folder.

You can import OOTB logical rules from the below location.

<NX Installation Location>\MBD

You can import these rules using the below offline utility.

<NX Installation>\RULE\nxmanager\tcin_logicalrule_setup.bat

You can also import the logical rules using NX UI dialog, using "Import Assembly into Teamcenter".

While importing please make sure that you are only selecting rules. (By setting "All Files")  


Now if you select "More" option, this will display the above imported logical rules.


KB Article ID# PL8704592

Contents

SummaryDetails

Associated Components