Solid Edge Solid Edge 2022 - Maintenance Pack 12 Announcement

2023-03-06T22:44:18Z
SE_BETA SE_TSS DOC_MANAGEMENT FLOEFD 3D-SKETCH SIMULATION Teamcenter Share TECH_PUB ASSEMBLY APPLICATION PART/SHEETMETAL TRANSLATORS DRAFT SETUP Solid Edge Marketing

Summary


Details

March 6, 2023

Dear Solid Edge Customer:

Solid Edge 2022 Maintenance Pack 12 is now available for download.

We appreciate your continued business and participation in the software support process - - your reporting helps us make Solid Edge more productive for how you do business.

Sincerely,

The Solid Edge Team

============

Release Notes:

============

Solid Edge 2022 MP12

Version: 222.00.12.04

Solid Edge 2022 Maintenance Packs are delivered using Microsoft Installer (MSI) technology.

Support Center: https://support.sw.siemens.com

===============

Email Notification:

===============

To receive direct email notifications for Solid Edge Maintenance Packs, navigate to your Support Center profile:

https://account.sw.siemens.com/profile, scroll down to Newsletter Subscriptions, then check the box for 

Software Field Bulletin

============================================

This Maintenance Pack addresses the following PRs:

============================================

===API===

PR 10520894: Automation oOccs.AddByFilename is not honoring the "flexible hose" settings

===Assembly===

PR 10453306: Fastener System all lengths of screws in selection mask

PR 10475009: Holding the control key does not work with a mixture of Designed/Simplified Assemblies

Eric - PR 10498699: Solid Edge doesn't retain assembly display options

PR 10503112: Some Parts with features on them do not display

PR 10510151: Locate filter does not remember cylindrical faces

PR 10541086: Solid Edge crash while working in Electrical Routing

PR 10543096: mirror option does not reflect feature updates in the parent assembly

PR 10591040: Open Assembly model breaks relationship creation

PR 10484946: A mismatch between the TC BOM view and the Solid Edge structure in AP Assembly

PR 10495507: adjustable parts are not correctly recomputing when saving an alternate assembly file

PR 10592376: "Physical Properties" command causes Solid Edge to crash.

PR 10594324: Piping Route using chain selection not working for 2D sketches.

PR 8626476: Some Adjustable parts are showing up in their original state

PR 8665618: Visible Faces command leads to the wrong representation of Frame-Elements.

PR 8633765: Chain selection for Tube in XpresRoute not working for 2D Sketches ( 10450645)

PR 8645790: Please repair in 2022 - This Assembly Crashes when deleting a frame component

PR 8670879: Some pattern feature instances go missing

PR 8671425: Adjustable tubes not getting created/updated correctly

===Draft===

PR 10482064: Crash after deleting block selected with Bottom-up locate

PR 10590299: Embedded solid edge text is not updating without save

PR 8670812: In a weld symbol, the note should not appear if the tail option is set to None

===Part/Profile/Sheetmetal===

PR 10531640: Abort when connecting Curve to 3D Sketch

PR 8641346: Equation Driven Curve does not consider Units from Variable Table.

PR 8653590: Quick Pick makes Solid Edge Crash

PR 251891: Abort on starting Blank Command in Dev Release

===Simulation===

PR 10498442: Unable to create a simulation report for an assembly that contains a weld

===Data Management===

PR 10534338: Design configurator in SE 2022 does not work since 1-01-2023

PR 8633957: Solid Edge data management not usable in production environments

===Embedded Client===

PR 10221766: Replace Revision does not work correctly with Multiple Revisions enabled

PR 10386780: Dispatcher support is failing to create/upload PDFs

PR 10472528: Revise through Structure Editor creates Multiple Datasets

PR 10490517: Solid Edge crashes when opening a file

PR 10501931: art occurrences are being replaced in assembly.

PR 8648840: SE crash when using replace function

===Translators===

PR 10496846: Fraction Bar Missing.

PR 10160786: Problem with chamfer

===TechPubs===

PR 10401428: Missing or faded PMIs when publishing a 3D PDF with section views

KB Article ID# PL8703632

Contents

SummaryDetails

Associated Components

SE_BETA