Cannot Output Operator Message when using Local Return

2023-03-15T13:20:33Z

Summary


Details

A Turning operation is created to rough a part. The material is difficult to machine so the Local Return option is used to periodically change the cutter inserts. At a set interval the tool will retract to a safe position, Stop the machine and display an Operator Message. When posted, though, the Operator Message is missing. What can be done to output this text?



Platforms
  • na windows-1064
Release Versions
  • NX V2212
Solution

Adding an Operator Message to the Start of Path Events caused the Local Return Operator Message to be output.



Notes

This issue is reported to be fixed in NX2306.

KB Article ID# PL8703605

Contents

SummaryDetails

Associated Components