Setting the default modelling mode in Solid Edge

2023-04-20T14:24:26Z

Summary


Details

Setting the modelling mode in Solid Edge between ordered and synchronous.

Solution

To set the default modelling mode for Solid Edge Part and Sheetmetal models, start Solid Edge.

Select "File" from the menu then select Settings -> Options -> Helpers. There you will find radio buttons for both "Synchronous" and "Ordered". The current default setting will be selected. Select the desired mode with which new Part and Sheet Metal documents will start.

KB Article ID# PL8702030

Contents

SummaryDetails

Associated Components