Solid Edge 2023 Update 0003 Announcement

2023-02-25T16:08:41Z

Summary


Details

February 25, 2023

Dear Solid Edge Customer:

Solid Edge 2023 Update 0003 is now available for download.

We appreciate your continued business and participation in the software support process - - your reporting helps us make Solid Edge more productive for how you do business.

Sincerely,

The Solid Edge Team

============

Release Notes:

============

Solid Edge 2023 Update 0003

Version: 2210.0003.004 x64

Download Solid Edge 2023 (v2210) Updates

Note: if the direct download URL doesn't resolve in your browser, please navigate from the top-level Support Center.

===============

Email Notification:

===============

To receive direct email notifications for Solid Edge Updates, navigate to your Support Center Profile (https://account.sw.siemens.com/profile, scroll to Newsletter Subscriptions, and check the box for Software Field Bulletin

==========================================

This Solid Edge Update resolves the following PRs:

==========================================

===Assembly===

PR 10452416: Unable to edit a Fillet assembly feature

PR 10510151: Locate filter does not remember cylindrical faces

PR 10534555: Can't use Edit Definition with the Keypoint Curve Segment command

PR 10540510: Display issues with multiple AMD Radeon Pro graphic card models and SE2023

PR 10541086: Solid Edge crash while working in Electrical Routing

PR 10543096: The mirror option does not reflect feature updates in the parent assembly

PR 10495507: Edit adjustable part in Alternate Assembly will modify all instances

PR 10586496: Isolate should work for multiple selected components

PR 10484946: A mismatch between the TC BOM view and the Solid Edge structure in AP Assembly

PR 10492607: Solid Edge parts cannot be assembled

PR 10517380: Frames not shown anymore; only the "Base parts" are visible

PR 10533761: Mirrored sub does not reflect changes in the parent

PR 10540510: Display issues with multiple AMD Radeon Pro graphic card models

PR 10580549: The user is not able to place a feature on a part in this file

PR 10581649: Changes to a part in a subassembly are not being reflected at top level assembly

PR 10592376: "Physical Properties" command causes Solid Edge to crash

PR 10594941: CTRL+C does not work in the Peer Variable Table

PR 10595062: Center-plane relationships to reference plane do not update

PR 8626476: Some Adjustable parts are showing up in their original state

PR 8631708: CoV/CoM changes from the Physical Properties dialog do not show up on the screen

PR 8665618: Visible Face command leads to the wrong representation of Frame-Elements

PR 9501471: Deactivated parts not being included when performing a Save As to a new document

PR 8671425: Adjustable tubes not getting created/updated correctly

PR 244715: Crash in Context Toolbar

===Draft===

PR 10535828: Text Boxes cannot be selected with the Line Up Text command in 2023

PR 10518174: Regression in Text box numbering

PR 10582309: The user is having a problem accessing the Solid Edge Inspector

PR 10401428: Missing or faded PMIs when publishing a 3D PDF with section views

PR 8670812: Weld symbol note should not appear if the tail option is None

===General===

PR 10497391: When running Solid Edge 2023 with a cloud license, Keyshot opens in DEMO mode

===Part/Profile/Sheetmetal===

PR 10540613: Move Faces Along 2 Point Vector issue, regression against SE2022

PR 10586927: Can't change direction (Extent Step) in Extrude

PR 10588722: Moving a hole by using dimension with Auto solution manager causes a crash

PR 8653440: Hybrid (synch and ordered) model modifying issue

===Data Management===

PR 10490546: Design Manager does not start when 2ddrafting is in a License File

===SEEC===

PR 10386780: Dispatcher support is failing to create/upload PDFs

PR 10528414: Dynamic Visualization makes Solid Edge Crash

PR 10308897: Replace or add a new line generates a new find number for an existing part in BOM

PR 211505: Changing SEStatus property does not prompt to save the change

===Translators===

PR 10496846: Fraction Bar Missing

PR 10160786: Problem with chamfer

PR 10491545: Crash while opening this Parasolid file

===TechPub===

PR 10537421: Back View command doesn't work in Solid Edge Illustrations 2023

PR 10594513: Parts List command fails to launch the selected parts list in the Model tab

KB Article ID# PL8701782

Contents

SummaryDetails

Associated Components