Solid Edge property with type String not converted to Number

2023-02-24T14:59:30Z

Summary


Details

I would like synchronize a Solid Edge PMI dimension with a property Teamcenter.

To do that, I expose the dimension PMI in a Solid Edge property and map the exposed variable to a Teamcenter property with the type "Number".

When I upload the file to Teamcenter, I get error message, below:


Platforms
  • na windows-1064
Release Versions
  • Solid Edge V223UPD2
Solution

To resolve this problem, you need to create a scalar type variable with formula linked to the PMI variable

This will remove the units from the custom property.


Consequently, you are able to synchronize the properties to Teamcenter without a warning.



Notes

KB Article ID# PL8701014

Contents

SummaryDetails

Associated Components