How to turn OFF the "No Teamcenter Classification..." message for all users

2023-03-31T12:11:51Z

Summary


Details

When adding a Material (Tools --> Material --> Assign Material) to a body the message: "No Teamcenter Classification license or NX Access Teamcenter Classification license." is returned.

In NX7.5.2.5 MP3 RevA and NX7.5.3.3 the Material Library began using the TC Classification, as such it has been integrated into the Reuse Library code. However it is not part of the Reuse Library.

This message can be turned OFF so that users do not see it when needing to add a Material to a body.

Platforms
  • INTEL windows-XP32_SP2
Release Versions
  • NX V7.5.3
Solution

Remove the following from the Customer Defaults:

Remove the Classification library setting in Customer Defaults --> Gateway --> Reuse Library --> General tab --> Libraries organized by Classification (list box), delete the OOTB setting - "Classification Root|ICM".

This will prevent users from having to acknowledge the message each time or select the "Do Not Display This Message Again" for the warning pop-up.

Notes

KB Article ID# PL8698749

Contents

SummaryDetails

Associated Components