OPC UA mapped signals, but they still do not update.

2023-02-22T17:41:37Z

Summary


Details

In Process Simulate, established connection to OPC UA, mapped signals, but they still do not update.

Platforms
  • na windows-1032
Release Versions
  • Tecnomatix V2206.X
Solution

Make sure the signal name and namespace are correct; on the connection settings it is better to select a signal tag (not a folder/category) for Process Simulate to indicate the proper namespace. For OPC UA, it is possible that the signal names in Process Simulate need to be between quotes. For example: "I1".

Notes

KB Article ID# PL8698733

Contents

SummaryDetails

Associated Components