NX Menu button and the top border bar are missing from the NX UI

2023-02-13T12:32:01Z
NX for Manufacturing

Summary


Details

After installing a new version of NX, the user reports that the Menu button and the top border bar under the ribbon are missing.

Solution

In a new default installation, NX runs with a simplified UI.  In the NX session, go to the Roles tab on the Resource Bar and choose one of the Advanced roles, such as "CAM Advanced" for a manufacturing user.  This will show the Menu button and its border bar, as well as all the extended ribbon bar icons the user is expecting to find.


Notes

Reference the NX2212 Help page on roles:

https://docs.sw.siemens.com/en-US/doc/209349590/PL20220512394070742.customizing_nx_installation/roles_ov

KB Article ID# PL8697772

Contents

SummaryDetails

Associated Components

Manufacturing General