While in the Drafting application, the Note command is missing the options to insert a Part Attribute, or Expression.
This is also missing when going to 'Edit Text' in the cell of a table, Tabular Note.
When in a drawing and inserting a Note, the Text dialog will appear, but the missing options are now moved to the ribbon toolbar.
While in the Text dialog, the user is placed into the 'Text General' tab on the ribbon. This tab of the ribbon has the options to insert a Part Attribute, insert an Expression, insert a Symbol, etc. The user can use these options from the ribbon while in the Text dialog.
Notes